July 2, 2013

              USB 3.0 Accessories from Basler – Tested, Reliable, and Cost-efficient

              USB 3.0 card and cable

              USB 3.0 card and cable

              The new USB 3.0 technology keeps system setup simple while delivering strong value for the performance – including for accessories. There are significant differences between accessories for machine vision applications and USB 3.0 products for the consumer market. The use of components tested and approved by Basler ensures a stable system setup, which in turn boosts cost efficiency.

              We are currently offering the following accessories for the Basler ace with USB 3.0 interface:

              • USB 3.0 cable with Micro B plug on the camera side and a USB 3.0 A plug on the host side – 3 m
              • USB 3.0 cable with Micro B plug on the camera side and a USB 3.0 A plug on the host side – 5 m
              • USB 3.0 card with 1 lane and 2 ports
              We will soon be adding a industrial-strength USB 3.0 hub with 4 ports for setups with more than two cameras.

              Have you visited our accessories database?

              You can review our entire catalog of cables, lenses, cards, switches, etc. under Cameras/Accessories. Once inside the database, simply select the preferred category of accessory and/or your Basler camera and you'll be presented with a convenient list of all available components.

                RSS Feed

                Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
                RSS News Feed
                 
                Please activate cookies in order to download files without having to fill in your data again the next time you visit.