January 8, 2015

              The New pylon 4 Winter Release is Now Available!

              pylon Winter release

              The new version 4.2.1 of the pylon 4 Camera Software Suite is now ready for download. This version includes a preview for the new Easy SDK for Windows .NET languages (C#, VB.NET, etc.) and an Automatic Adjust Image function within the pylon Viewer.

              The Easy SDK and its new .NET API deliver a generic, uniform programming interface for all Basler cameras. This means for example very simple migration from one camera interface to another without major changes to the code. The Easy SDK also offers a collection of .NET WPF controls that can be put together into a custom pylon Viewer in just a few minutes using the mouse — without having to write a single line of code. Our new screencast video shows how it works!

              Another attractive feature is the new Automatic Adjust Image button in the pylon Viewer. A single click on this button triggers automatic configuration of the selected camera to its environment in terms of color and brightness.

              You can find more information about the pylon 4 Winter Release here.

              Please feel free to contact our Basler Support Team if you have any questions or need additional information.

                RSS Feed

                Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
                RSS News Feed
                 
                Please activate cookies in order to download files without having to fill in your data again the next time you visit.