October 12, 2015

              Production Automation for Medical Device Manufacturing – with the Basler dart Camera

              Production automation for medical device manufacturing – with the Basler dart camera
              Vision systems with digital cameras are becoming more and more important for medical applications. Whether it is diagnosis and patient treatment, or production of medical devices and components, vision systems can be very useful. As applications grow in their complexity, system precision and reliability become ever more important.

              The Finnish company Ginolis has designed a modular desktop robotic production cell. It can help their customers to automate the respective production processes for manufacturing high-precision in-vitro diagnostic disposables. Ginolis chose the Basler dart board level camera because of the small footprint e.g. of 27 mm x 27 mm for the bare board version, as well as due to its different optical mount options. This camera grants high flexibility for the system integration.

              Read more in the following success story:

              RSS Feed

              Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
              RSS News Feed
               
              Please activate cookies in order to download files without having to fill in your data again the next time you visit.