March 17, 2014

              NIR Cameras Used to Deliver Only the Freshest Fruits and Veggies

              Basler NIR Cameras
              Everyone has at one time or another bought a seemingly pristine piece of fresh fruit, only to discover pressure damage on it the next day. These blemishes often enrage consumers, who feel cheated because they can't see the problem in advance. Fruit and vegetable producers want to offer consumers flawless products. Their only hope for this is inspecting for hidden bruises on the inside of the fruit as well.

              NIR cameras are a strong tool in detecting damaged spots under the peel that are invisible under normal light. Cameras equipped for this application can be integrated into sorting lines to help sort fruit more effectively into different quality classes. For end consumers, the benefits are clear: Fruit that looks as good at home as it did in the store.

              Basler offers special cameras with NIR-optimized sensors for this type of application. A breakthrough in CMOS technology makes it relatively easy from a technical standpoint to produce sensors with heightened sensitivity in the near-infrared range above 850nm, all at affordable prices. The boosts to NIR sensitivity in these CMOS sensors comes thanks to a novel manufacturing method. The thickness of the substrate film on the sensor chip is increased compared with the parameters on normal monochrome sensors. Thanks to the new CMOS technology, more and more of this new generation of industrial cameras with very good sensitivity are entering the industrial machine vision market. Basler is proud to offer these cameras at an attractive price.

              Visit our website for an interesting article on the topic of NIR cameras. 

              Interested in learning more about Basler cameras with NIR-optimized sensors? Our sales team would be glad to assist you.

                RSS Feed

                Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
                RSS News Feed
                 
                Please activate cookies in order to download files without having to fill in your data again the next time you visit.