October 11, 2012

              New: Edge Storage in all Basler IP Cameras

              Basler IP Camera with SD Card Slot

              The SD card functionality already available in Basler IP Fixed Dome Cameras will now also be integrated into our IP box camera range.

              In this setup, the microSDHC card slot provides for local storage of up to 32 GB of data. This functionality makes it possible to store live streams or single camera images in configurable time intervals on an SD card. If a network failure occurs, the camera acts as a backup solution by recording video streams to the SD card. When the network connection has been restored, the video management system can retrieve the data and merge it seamlessly with video footage captured before the connection was interrupted.

              When using an efficient encoder type such as H.264 and a high-capacity SD card, a Basler IP Camera can independently capture and store images for an extended period of time without transmitting data back to a client. This is especially useful in remote surveillance locations, since the camera will not require any network connection.

              “With edge storage, our IP cameras can act as self-sufficient systems,” states Björn Weber, Product Manager at Basler. “Our customers can rely on uninterrupted video footage even in case of network failures.”

              Basler IP Cameras are available as box and dome models with resolutions of VGA to 5 megapixels and frame rates of up to 100 frames per second.

                RSS Feed

                Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
                RSS News Feed
                Please activate cookies in order to download files without having to fill in your data again the next time you visit.