July 20, 2016

              First Design-In Samples Now Available: New ace Models with Sony's IMX 250, 252, 264 and 265 Sensors

              Design-in samples are now available for five new ace USB models featuring Sony's IMX 250, 252, 264 and 265 sensors. The five new cameras offer resolutions from 3.2 to 5 megapixels and frame rates of up to 120 fps.

              Thanks in part to pixels measuring just 3.45 µm, the sensors deliver strong sensitivity, low noise levels and very good overall image quality at high resolution and fast frame rates. They are also capable of sensing light in the near-infrared range. Many applications, from electroluminescence inspections to traffic and security applications, require only low levels of sensitivity in this spectrum and work effectively even without a dedicated NIR sensor.

              In addition to the speedy sensors IMX250 and IMX252 Sony has positioned a counterpart for each sensor with a lower frame rate, just as they did with the IMX174. These sensors — the IMX264 and IMX265 — represent economical alternatives capable of producing the same image quality, but with lower frame rates. They are the perfect choice for applications that do not require extreme high-speed image acquisition. For this reason, Basler provides the faster sensors IMX250 and IMX252 in combination with the USB 3.0 interface. Unlike GigE, USB 3.0 offers the bandwidth needed to properly service the higher frame rates of the IMX250 and IMX252. The decision not to offer GigE variants of the IMX250 and IMX252 was a conscious one, as the more economical IMX264 and IMX265 sensors already perform better than their more expensive GigE counterparts could do.

              Beyond this, the sensors are also notable for their small dimensions, allowing them to work in combination with economical 2/3" lenses.

              Taken as a whole, these properties make the new IMX sensors ideal partnersfor Basler's most successful series of cameras, the ace line. In all, twelve ace models are planned with the new IMX 250, 252, 264 and 265 sensors from the Pregius series by Sony.

              Design-in samples are now available for the camera models:

              Model

              Resolution

              Speed

              Sensor

              Mono/Color

              Interface

              acA2040-55um

              3.2 MP

              55 fps

              IMX265

              Mono

              USB3

              acA2040-120um

              3.2 MP

              120 fps

              IMX252

              Mono

              USB3

              acA2440-35um

              5 MP

              35 fps

              IMX264

              Mono

              USB3

              acA2440-75uc

              5 MP

              75 fps

              IMX250

              Color

              USB3

              acA2440-75um

              5 MP

              75 fps

              IMX250

              Mono

              USB3

              Upcoming design-in samples (planned for 3Q-4Q 2016):

              Model

              Resolution

              Speed

              Sensor

              Mono/Color

              Interface

              acA2040-55uc

              3.2 MP

              55 fps

              IMX265

              Color

              USB3

              acA2040-120uc

              3.2 MP

              120 fps

              IMX252

              Color

              USB3

              acA2440-35uc

              5 MP

              35 fps

              IMX264

              Color

              USB3

              acA2040-35gm

              3.2 MP

              35 fps

              IMX265

              Mono

              GigE

              acA2040-35gc

              3.2 MP

              35 fps

              IMX265

              Color

              GigE

              acA2440-20gc

              5 MP

              20 fps

              IMX264

              Color

              GigE

              acA2440-20gm

              5 MP

              20 fps

              IMX264

              Mono

              GigE

                RSS Feed

                Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
                RSS News Feed
                 
                Please activate cookies in order to download files without having to fill in your data again the next time you visit.