February 3, 2013

              Cables With Protective Circuit for ace Camera Link Models

              Basler offers you an extensive selection of camera accessories. For the Basler ace area scan cameras with Camera Link interface we've added a 5 and 10-meter Power-I/O cable with M5 4pin plug to the portfolio, among other items.

              The 10-meter cable is also outfitted with a protective circuit to let it be used with a PLC (programmable logic controller). Unlike traditional cables, this one offers you a protective circuit, meaning:

              • Adaptation of the PLC voltage to the TTL voltage of the camera
              • Protects the camera against reverse voltage
              • Protects the camera against alternating voltage
              The direct triggers for the ace CL cameras avoid undefined signal delays through the reaction time of the PLC or frame grabber. This is essential for true harnessing the high refresh rates of our ace Camera Link models - up to 340 images per second.

              Visit our accessories database to view all of the available components for your Basler camera. Simply select the camera series or models or the accessory category, such as cable or lens, and you’re ready to go.

                RSS Feed

                Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
                RSS News Feed
                Please activate cookies in order to download files without having to fill in your data again the next time you visit.