March 17, 2016

              Basler will reveal BCON at The Vision Show in Boston

              Basler will reveal BCON at The Vision Show in Boston
              The Vision Show, organized by the machine vision association, AIA, will take place on May 3-5, 2016 at the Hynes Convention Center in Boston. It is the main event for the vision industry in the Americas for this year and Basler is taking part in it.

              At booth 803 we will present the newest addition to the dart board level camera family, the dart BCON. BCON is a unique interface developed by Basler based on the LVDS (Low Voltage Differential Signaling) standard. It offers reliable image data transfer at high speed. The BCON interface offers the highest flexibility for connecting with LVDS-based technology, like FPGA (Field Programmable Gate Array) boards and SoCs (System on Chip).

              Another show highlight will be the new Basler ToF camera, the first high-resolution Time-of-Flight camera on the market, offering 3D technology suitable for the mass market.

              Also on the show floor there will be the new Basler ace models with Sony’s IMX174 and IMX249 sensors and the PYTHON sensors from ON Semiconductor. These cameras already come with Basler's new PGI feature set which achieves improved sharpness, denoising, color-anti-aliasing, and 5x5 debayering.

              In addition, there will be the pulse and the Basler beat camera series as well as the Basler Lenses on display.

                RSS Feed

                Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
                RSS News Feed
                 
                Please activate cookies in order to download files without having to fill in your data again the next time you visit.