June 17, 2015

              Basler ace USB 3.0 Cameras and Basler pylon Camera Software Suite Support Research in Cell Biology

              Microscopy is a key component of research in cell biology. It's an essential factor in optical inspections of even the smallest cells. While microscopes are used to create the images, high-quality cameras and suitable software are needed to process them digitally. Dartsch Scientific, an institution for test systems for cell biology, uses two Basler ace USB 3.0 cameras and the Basler pylon Camera Software Suite for this task. 

              The Basler cameras have two missions: one of the two cameras is used as a highly effective tool for capturing rapid cell movements. The other camera makes a constant recording of the cell behavior. With the aid of the pylon Viewer, the desired images can then be extracted for further processing.

              For more details on the cell research at Dartsch Scientific and the use of Basler ace USB 3.0 cameras and pylon software, please see our Success Story "Progress in Cell Biology Research with Basler ace USB 3.0 Cameras and the Basler pylon Camera Software Suite" in the Download area.

              RSS Feed

              Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
              RSS News Feed
               
              Please activate cookies in order to download files without having to fill in your data again the next time you visit.