Glossary

1080p

1080p is short form term designating a set of HDTV characterized by 1080 horizontal lines resolution and progressive scan.
more

5x5 Debayering

PGI debayering is a debayering algorithm developed by Basler that works with a 5x5 pixel radius.
more

720p

720p describes the lowest resolution defined in the television standard for High Definition TV.
more

ADC

An electronic device that converts a voltage to a proportional digital number.
more

Analog-to-digital converter

An electronic device that converts a voltage to a proportional digital number.
more

AOI

Area of Interest (AOI) - a portion on the camera's sensor.
more

AOI-Level 1

Support of certain resolutions (e.g. CIF, PAL etc.).
more

AOI-Level 2

Support of any resolution, configuration via WebInterface only.
more

AOI-Level 3

Support of any resolution, configuration via WebInterface or video management software.
more

AOI-Level 4

Support of digital pan/tilt by moving an AOI.
more

AOI-Level 5

Support of output scaling configuration via video management software.
more

API

Application Programming Interface (API) - a set of specifications allowing application software to communicate with the camera.
more

Area of Interest

A portion on the camera's sensor.
more

Area of Interest (AOI), also known as Region of Interest (ROI)

Defines the sensor's area of detail used to capture the image.
more

Area Scan Camera

Area Scan cameras contain a rectangular sensor with more than one line of pixels, which are exposed simultaneously.
more

Bayer BG 12 / Bayer GB 12

Data format for transfer of image data for color cameras with 12 bits of data per pixel, embedded in 16 bits.
more

Bayer BG 12 Packed / Bayer BG 12 p

Format for data transmission for color cameras with 12 bits of data per pixel, with 2x12 bits packed into 3 bytes.
more

Bayer BG 8 / Bayer GB 8

Data format for transfer of image data for color cameras with 8 bits of data per pixel.
more

Bayer pattern

A regular array of red, green and blue color filters covering a sensor's pixels.
more

Binning

Technique of summarizing several neighboring pixels in the sensor of an industrial camera to a block of pixels with the goal of improving the signal to noise ratio.
more

Blooming

An artifact occurring in images that were acquired by a CCD image sensor.
more

C-Mount

A lens mount for screw in lenses.
more

Camera Link

Camera Link (CL) is a serial communication protocol designed for computer vision applications.
more

CCD

A charge-coupled device (CCD) is a device for movement of electrical charge.
more

CCD Sensor

Electronic device to convert light (photons) into electronic signals (electrons).
more

CCT+

The Basler Camera Configuration Tool Plus (CCT+) is a Windows based tool for configuring Basler cameras that adhere to the Camera Link standard.
more

Charge-Coupled Device

A charge-coupled device (CCD) is a device for movement of electrical charge.
more

CMOS

Complementary metal-oxide-semiconductor (CMOS) is a technology for constructing integrated circuits.
more

CMOS Sensor

Electronic device to convert light (photons) into electronic signals (electrons).
more

Color Creation

more

Color filter

Colored transparent cover for a pixel.
more

Color Interpolation

Refers to the method of calculating full color information for a pixel.
more

Color-Anti-Aliasing

Color-Anti-Aliasing reduces and corrects color errors and discolorations.
more

CS-Mount

A lens mount for screw in lenses.
more

Day/Night Functionality

Provides clear camera images even in low light.
more

Debayering

Ensures that image colors are correct; uses an algorithm to reconstruct the color values of the mosaic created by the color sensor.
more

Denoising

PGI executes all computational steps needed to process a raw image into a finished color image in parallel instead of sequentially, thus avoiding an excessive amplification of noise.
more

Design-in sample

Basler design-in samples are early versions of products. They can be used to evaluate a product’s basic performance and consider if it is suitable to be integrated into an application.
more

DirectShow

DirectShow is a standard established by Microsoft for the exchange of data between audio and image sources (such as a digital camera, microphone or files) and programs for Microsoft Windows.
more

DNS

Domain Name System
more

Dynamic Range

Dynamic Range describes the ratio of the largest signal to the smallest signal (that can be distinguished from noise) in an image.
more

EMVA

The European Machine Vision Association (EMVA) is an association of companies and corporations involved in machine vision and standardization in that field.
more

EMVA1288

The EMVA1288 standard describes a unified method to measure, compute, and present the specification parameters for cameras and image sensors used in machine vision applications.
more

Ethernet

Ethernet is a family of computer networking technologies for local area networks (LANs) commercially introduced in 1980.
more

European Machine Vision Association

The European Machine Vision Association (EMVA) is an association of companies and corporations involved in machine vision and standardization in that field.
more

Event Reporting

Allows the camera to report events to make it easier for the PC to control image capture.
more

Exposure Active Signal

Digital signal from the camera to control image capture.
more

F-Mount

A bayonet type lens mount.
more

Fixed Box Camera

Fixed camera e.g. for video surveillance.
more

Fixed Dome Camera

Fixed camera with dome housing.
more

Flash Window Signal

Digital signal from the camera to control external illumination.
more

FPS

Unit of the frame rate.
more

Frame Grabber

An electronic device installed in a PC for interfacing to a camera.
more

Frame Rate

The number of frames per second that are acquired or transmitted.
more

Frame Start Trigger Delay

Function to delay image capture.
more

Frames per Second

Unit of the frame rate.
more

Full HD

A set of HDTV characterized by 1080 horizontal lines resolution and progressive scan.
more

Full well capacity

This quantity refers to the largest charge that a pixel can hold before an overflow of charge into adjacent pixels within the sensor causes the so-called blooming.
more

GenApi

An API for configuring machine vision cameras
more

GenICam™

GenICam is a standard of the European Machine Vision Association (EMVA) allowing to control machine vision cameras via a generic programming interface.
more

GenTL

A module of GenICam providing a unified mechanism for grabbing and streaming images from the camera.
more

Gigabit Ethernet

Gigabit Ethernet (GigE) defines a tethered protocol for data transfer based on the widespread Ethernet standard.
more

GigE Vision

GigE Vision is an interface standard for industrial image processing by digital cameras that originated in the field of machine vision.
more

H.264

Standard for video compression.
more

HD

The lowest resolution defined in the television standard for High Definition TV.
more

High Profile

A specific H.264 profile.
more

IEEE1394 (FireWire)

FireWire or IEEE1394 is a bus standard for serial data transmission.
more

IEEE1588 (PTP)

The Precision Time Protocol (PTP), also known as IEEE 1588, is a network protocol,  responsible for the synchronization of clocks on multiple devices within a computer network.
more

Image Sensor

An electronic device containing a large number of small light sensitive areas (pixels), where photons generate electric charges that are transformed to an electric signal.
more

Improved Sharpness

PGI works with an interpolation algorithm that is adapted for the image structure and can thus deliver significantly improved sharpness.
more

Interlaced scan

Readout of an image sensor or update of an image frame occurs in an alternating fashion for odd-numbered and even-numbered horizontal lines of pixels.
more

Internet Protocol

The Internet Protocol (IP) is the principal communications protocol used for relaying datagrams (packets) across an internetwork using the Internet Protocol Suite.
more

Internet Protocol address

Unique address in a network.
more

IR-cut filter

An infrared cut filter (IR-cut filter) is used to block light with wavelengths longer than visible light while transmitting visible light.
more

Line Scan

Line Scan cameras have a sensor consisting of 1 to 3 pixel lines.
more

Mono 12

Data format for transfer of monochrome image data with 12 bits of data per pixel, embedded in 16 bits.
more

Mono 12 Packed / Mono 12 p

Format for data transmission for monochrome cameras with 12 bits of data per pixel, with 2x12 bits packed into 3 bytes.
more

Multi-Streaming and Multi-Encoding

more

Multicast

Multicasting allows an IP camera to simultaneously transmit images to multiple devices attached to the network.
more

OEM

An original equipment manufacturer (OEM) manufactures products or components.
more

Original Equipment Manufacturer

An original equipment manufacturer (OEM) manufactures products or components.
more

PGI

The PGI Feature Set is an in-camera image optimization developed by Basler.
more

PoE

PoE (Power over Ethernet) technology describes a system to pass low voltage electrical power safely, along with data, on Ethernet cabling.
more

Power over Ethernet

Power over Ethernet (PoE) technology describes a system to pass low voltage electrical power safely, along with data, on Ethernet cabling.
more

Primary Colors

A set colors from which other colors can be derived.
more

PTP

The Precision Time Protocol (PTP), also known as IEEE 1588, is a network protocol,  responsible for the synchronization of clocks on multiple devices within a computer network.
more

pylon

The Balser pylon Camera Software Suite is a collection of drivers and tools for operating any Basler camera.
more

RoHs

Collective term for Directive (European Union) 2002/95/EG and its realization into national right.
more

SDK

Software Development Kit
more

Sensor

An electronic device containing a large number of small light sensitive areas (pixels), where photons generate electric charges that are transformed to an electric signal.
more

Sequencer

Applies a series of pre-defined configuration steps to a series of captured images.
more

Signal-to-Noise Ratio

A measure that compares the level of a desired signal to the level of background noise.
more

TCP

Transmission Control Protocol
more

TWAIN

TWAIN (Technology Without An Interesting Name) is a standard defined by a coalition of companies for the exchange of data between image input devices, such as digital cameras (like those from Basler) and programs for Microsoft Windows and Apple Macintosh.
more

UDP

User Datagram Protocol
more

Unicast

Unicasting is the common capability that lets an IP camera transmit images directly to a single device attached to the network.
more

Vandal resistance

Ability to withstand deliberate attempts of damage.
more

VBR

Variable Bit Rate
more

VGA

A graphics card driver standard.
more

Video Graphics Array

A graphics card driver standard.
more

VoIP

Voice over IP
more

White Balance

The white balance helps to adjust a color camera to the ligting conditions.
more

 
Please activate cookies in order to download files without having to fill in your data again the next time you visit.